AXIS#.IL.FOLDFTHRESHU
Description
AXIS#.IL"Instruction list" This is a low-level language and resembles assembly.FOLDFTHRESHU is the fault level of the current foldback algorithm. The value of AXIS#.IL.FOLDFTHRESH is the minimum of AXIS#.IPEAK , AXIS#.MOTOR.IPEAK , and AXIS#.IL.FOLDFTHRESHU.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
General Information
|
Type |
Read/Write |
|
Units |
Arms |
|
Range |
0 to 500 Arms |
|
Default Value |
Drive peak current (IPEAK) |
|
Data Type |
Float |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.IL.FOLDFTHRESHU | 0x500A | 0x9 | DINT | 1000:1 | - | RW | False |
| AXIS2.IL.FOLDFTHRESHU | 0x510A | 0x9 | DINT | 1000:1 | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|